STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Assistance with Debugger Issue

Hi all, I've been battling a frustrating issue on my STM32F407 Discovery board for the past few days. I don't know where the fault lies exactly but hopefully if I explain someone can point it out. I'm working on a robotics project, not doing anything...

GEvan.1 by Associate
  • 1330 Views
  • 1 replies
  • 1 kudos

1GB memory usage instead of 512MB for STM32L4R9AI

The STM32L4R9AI documentation says that it supports Macronix MX25LM51245GXDI00 and Micron MT35XL512ABA1G12-0SIT Octo-SPI Flash memories. These modules are not currently available for sale.Please tell me, is it possible to use MX66LM1G45GXDI00 instead...

VTeli.2 by Associate II
  • 6658 Views
  • 5 replies
  • 0 kudos

QSPI issue

I am using STM32F746 controller and MX25L128 flash on a custom board.I want to make external flash loader file for my custom board.I followed the MOOC - External QSPI loader how toI got error while memcmp for (var = 0; var < SECTORS_COUNT; var++) { ...

NMait.1 by Associate II
  • 1066 Views
  • 1 replies
  • 0 kudos

Resolved! How to use LCD MIPI DSI LP Mode to initialize LCD?

Hi Sir,I used STM32F469i-DISCO for evaluating my project.I now TRY LCD which driver IC is ST7701S and show some image in video mode at panel.ST7701s had to initialized in DSI LP Mode. I had referenced STM32Cube_FW_F4_V1.21.0 example projects. But I c...

CYong by Associate II
  • 3576 Views
  • 4 replies
  • 0 kudos

STM32F1xxx shortages

We moved to STM after being let down by Freescale and TI in terms of sourcing. We are now finding massive MCU shortages and lead times > 30 weeks. Even despite this, we just found out that apparently STM is not taking additional orders.It is frustr...

PKorz.1 by Associate II
  • 5434 Views
  • 13 replies
  • 3 kudos

WAKEUP from STANDBY mode and EXTI/NVIC IRQs

Hi all,I'm learning about low power modes , and I'm testing the RTC wakeup timer function.Datasheet talks about to set the IRQs for WakeUp timer on EXTI(IRQ 19) and NVIC(IRQ 3), but I tested in my code, with and without set these IRQs and the wakeup ...

JAlca by Senior
  • 1108 Views
  • 0 replies
  • 1 kudos

hello , im using adc-dac combination where i want to regenerate the waveform using dac. im fedding input to the adc externally using waveform generator. But the problem is my adc buffer show value beyoud 4000 irrespective of the input. why is this so.

even i grounded the ADC input pin but still i receive garbage values of >4000.Is there any problem with the configuration of adc. im currently stuck at the adc. anyone with the adc dac code help me out.