cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103RGT6 I2C state machine misunderstanding

fifi_22
Associate III

Hello.

I'm trying to get I2C working to read BMP280 sensor data. This is code I written so far:

	GPIOB->CRL |= GPIO_CRL_MODE6;				//set PB6 as output with drive strenght to 50Mhz
	GPIOB->CRL |= GPIO_CRL_CNF6;				//set PB6 to open-drain alternate function
	GPIOB->CRL |= GPIO_CRL_MODE7;				//set PB7 as output with drive strenght to 50Mhz
	GPIOB->CRL |= GPIO_CRL_CNF7;				//set PB7 to open-drain alternate function
 
	I2C1->CR2 |= 0x20;							//freq of cpu
	I2C1->CCR |= 0x80;
 
	I2C1->CR1 |= (I2C_CR1_PE);					//Peripheral enabled
 
	while (1){
 
		I2C1->CR1 |= I2C_CR1_START;
		while(!(I2C1->SR1 & I2C_SR1_SB));
		
		I2C1->DR |= 0x76<<1;
		while(!(I2C1->SR1 & I2C_SR1_ADDR));
		uint32_t asd = I2C1->SR2;
		
		I2C1->DR |= 0xD0;
		
		I2C1->CR1 |= I2C_CR1_STOP;
 
                //delay 1s
}

Code works nicely only once. It reads ACK from sensor (when sensor unplugged - no ack), but when it comes to send all of this one more time - it fails. Nothing gets sent and it stays in this loop: while(!(I2C1->SR1 & I2C_SR1_ADDR)); What I'm initializing not correctly? Is this a proper way to do I2C transfers on STM?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.