User Activity

Hi,I've developed a UI with touchGFX where I'm using a swipe container and to finish my application I think I need a way to know the page I was in the Swipe container. The steps I do are.:1) in page x of the swipe container i press a button to go to ...
Hi, which is the fastest way to migrate a touchGFX project from  STM32F746G-disco to STM32H735-DK? Actually on touchGFX application template I can't choose the STM32H735-DK. I will glad if someone could help me
Hi, I've created a custom keyboard and so far all works good. I've just a problem: I want to use an OK button on the keyboard to copy the text edited to a text area in an other screen. I'm able to go to the other screen but when i do the second part ...
Hi, I've already developed a graphic application with the STM32F746G-DISCO on TOUCHGFX and it works well.Now I would like to develop the same graphic application on a different ST board without an onboard TFT display. I want to use an external displa...