Question
strange debug ROM table entries
Hello,
I am looking into the ROM tables on STM32F439ZI.
TPIU (0xE0040000) class type is 0x9, in its romtable, there are two entries:
- 0xb, which is strange because it is marked as present (0b11) but offset is zero which is prohibited.
- 0x1, which means present value is 0b01, which is reserved.
ETM (0xE0041000) class type is 0x9, in its romtable, there is an entry:
- 0x411, which again has a present value of 0b01, which is reserved.
Am I mistaken or anyone can give insight what these are ?
Best regards,
Mete