STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am looking for working without hardware failure, testing report and status of obsolescence for 10 years and certification data.

Good Morning Sir,I am looking for working without hardware failure, testing report and status of obsolescence for 10 years and certification data. Part no of following component are:497-STM32L476ZGT6CT-ND497-BLUENRG-M2SPCT-NDSTC3100ISTM24M02-DRMN6TP4...

RJat by Associate
  • 777 Views
  • 0 replies
  • 0 kudos

STM32F469 SPI DMA repeat TX while filling RX buffer?

Hi thereI got an IC that needs to be fed with 32bit NOP words via SPI TX (0x00000000) to get 32bit data output via RX at the same time. Communication works fine in SPI polling mode but I really want to try to do it via DMA...My RX buffer is an array ...

0693W000008zC2SQAU.png
PGroe.2 by Associate III
  • 1721 Views
  • 2 replies
  • 0 kudos

HAL_Delay stuck in Loop

Hello!First of all, im pretty new to programming STMs. I'm currently working on a project on the WL Series and stuck with the HAL_Delay function. Even something super simple like toggling my User LED won't work.For RCC im using a TCXO 32Mhz as HSE.wh...

0693W000008ys3zQAA.png 0693W000008ys5MQAQ.png
GHube.1 by Associate II
  • 8074 Views
  • 6 replies
  • 1 kudos

Use of an external SDRAM (IS42S16320F) with STM32H753

Hello!I'm trying to use an external SDRAM (IS42S16320F) with an STM32H753 but no luck till now.Could please anyone check if my settings are correct because I don't know if I made a bug here.  For that I have attached the FMC configuration and the sch...

0693W000008yud1QAA.png 0693W000008yudBQAQ.png 0693W000008yudGQAQ.png
Gregory3 by Associate III
  • 7381 Views
  • 11 replies
  • 0 kudos

How can I use external SPI flash memory as a heap

Hello @All ALL​ ,@Martin KJELDSEN​ ,I am using STM32F412CGU6 Microcontroller.I would like to use external SPI flash memory as heap.Can you please give me some idea?Can you please suggest me the required changes in linker script?Is there any document ...

Resolved! Out-of-spec temperature behavior of STM32F412 (hard fault) ?

Hi all,I am testing product samples fitted with STM32F412RET6 which has a temperature operating range of -40°C +85°C.On some samples tested inside a climate chamber, the MCU unexpectedly reset due to cold temperature within operating range (e.g. -5°C...

MLiis.1 by Associate II
  • 3552 Views
  • 6 replies
  • 0 kudos