STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32476RG I2C mem write not seen in Memory read ?

Hi,Attached is the code where I am doing I2C write//I2C write in memory*/void I2C_write_mem(){ /*** Mac ID read I2C read***/  char MSG2[] = " start I2C3 write \n\r";       HAL_UART_Transmit(&huart5,(uint8_t*)MSG2,sizeof(MSG2),1000);       HAL_Delay...

RShiv.1 by Senior
  • 2261 Views
  • 4 replies
  • 0 kudos

May & Scolfield

Looking for samples please -6-8 pcsSTM32H743XIH6 / STM32H747XIH6Automotive - OEMKind RegardsRic

RBarr.4 by Associate
  • 785 Views
  • 0 replies
  • 0 kudos

How do I implement TCP/IP on the F746NG-Disco?

I referred to the example of 1.16.1 of F746G.The contents of MPU_Config() and System Clock_Config() have been copied. Ping test failed after applying rtOS (Stack Size = 256) and LWIP.The example is ping test, so there is no problem with the configura...

CHan.2 by Associate II
  • 758 Views
  • 0 replies
  • 0 kudos

How to set delay between two timers?

I have two signals, one I would like to output for the first 950 ms of every second and then a second signal that I would like to output at a variable start time of each second. I included my code (the delay function does not work) for reference if ...

SGold.3 by Associate II
  • 3694 Views
  • 8 replies
  • 0 kudos

Resolved! Stuck at HAL_init() with RAM.ld

Hi everyone!I'm using a nucleo H755 boardI'm basically trying to debug my code from RAM. I already set the linker to use the autogenerated ld file (STM32H755ZITX_RAM.ld). When I try to debug, the application initializes, however It does not go beyon...

GCanc.1 by Associate II
  • 1437 Views
  • 2 replies
  • 0 kudos