STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART DMA transmit and receive along with IDLE line detection

Hello,I'm trying to implement a UART DMA data transfer in STM32F429. I face the following problem.I'm using custom-made Python to receive and transmit data over the serial port. I am sending an unknown number of bytes from my computer to MCU. So, I'm...

ADani by Associate III
  • 1452 Views
  • 0 replies
  • 0 kudos

STM32G071C8T6 and USART3

Hi All,I don't managed to send char on USART3 with the attached project.I was wondering if someone had already detected issue in using USART3 Thanks in advance

gh_rcl by Associate II
  • 1810 Views
  • 3 replies
  • 0 kudos

Inconsistent CK_TIM18.. usage in reference manual

In the reference manual STM32H7 (version July 2018) in chapter 37.1 - figure 343 for the clock source it says "CK_TIM18 from RCC".Problem: If I look for "CK_TIM18" in the complete manual, this name appears ONLY ONE TIME, here in this chapter 37.1 fig...

flyer31 by Senior
  • 3660 Views
  • 9 replies
  • 0 kudos

STM32_PVD_need to set the reference Voltage

Hi i am using stm32H750VB as the IC for my project.I need to detect sudden power shutdown .I.e., i need to use PVD mode for detecting the sudden drop in voltage and save the EEPROM Contents.I need to use PVD using external analog voltage PIN RB7. But...

how to count pulses per interval

I want to count the number of pulses that occur in an interval controlled by a timer. I want to trigger the timer and the counter simultaneously. How can I do that?

pgregson1 by Associate III
  • 1209 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G431 Can't get DMA interrupts to trigger

Hi All,I please need your help as I have been stuck longer then I care to admit,I have a STM32G431 48-pin device which I am using TIM8 for input capture with DMA. I have an external input (PC6) for Ch1 input and am using a software trigger for Ch3.I ...

0693W00000AN5BoQAL.png
BTrem.1 by Senior II
  • 3092 Views
  • 7 replies
  • 0 kudos