STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

can't debug code using st link

Hi community @STTwo-32 ,I am using stm32f407vet6 board I am new to stm32 board.I wrote an Hello world program in STM32cubeide and i try to debug the code.I bought an ST-link v2 from online.when I try to debug the code it says frimware upgrade require...

Sabarinathan1_0-1752568379016.png Sabarinathan1_1-1752568635045.png Sabarinathan1_2-1752568705778.png

Option bytes all become 0xFF

The chip model we use is STM32L496VG. Our customer reported that the machine became unresponsive (bricked) and couldn't power on after an OTA upgrade. After receiving the machine, we used STM32 Programmer to read the flash, which prompted chip protec...

image-20250609-061456.png image-20250609-061443.png
Raysu by Associate II
  • 1723 Views
  • 7 replies
  • 6 kudos

eeprom emulation reliability - STM32H743I

 dear ST and/or Users, we’re using STM32H743I with a requirement now to store several bytes of data in non-volatile memory.  We have known-working code for the existing application, and need to be assured it is not affected when eeprom emulation code...

TMA1of3 by Associate III
  • 1061 Views
  • 5 replies
  • 2 kudos

Resolved! question about VDD pin

I'm a beginner and I don't understand the datasheet very well. Can I externally power my STM32 F446RE from the VDD pin (the one opposite E5V in the pinout)?Sorry for the banality, but I only found info for generic GPIOs.Dar

DAR20_01 by Associate II
  • 943 Views
  • 6 replies
  • 3 kudos

Resolved! STM32H7A3 stuck in SystemClock_Config in KEIL

I have a problem with an STM32H7A3 which remains stuck in SystemClock_Config. I use Keil. Any ideas please? it just remain stucked here: if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_Os...

laurianus by Associate III
  • 5556 Views
  • 13 replies
  • 2 kudos

Resolved! LCD display with LTDC for STM32H7

I'm trying to learn how to use the LCD display on the STM32H745I-DISCO board.(I'm a beginner at coding, so please go easy on me!) Right now, I'm just trying to display basic text on the screen, but nothing shows up, it's either all white or all black...