User Activity

Hi,I am using STM32N6570-DK kit. In my application I need ~3.5MB of RAM but if I allocate more than 256KB of RAM I get the error "region `RAM' overflowed by xxxx bytes".  I got the same results as well when I imported "UART_HyperTerminal_IT" example ...
Hi All,I want to plot the current state of the microcontroller at the same time. From what I understood it is possible using stm32CubeMonitor and STLINK-V3PWR. I have seen a similar dashboard in AN5999  but I couldn't find a way to create such a dash...
Hi All,I am working on a Dynamic graph widget on the STM32F7 board. Below is the configuration of my setup.1. Controller: STM32F756ZG 2. Display: Waveshare 7" LCD with 800x480 resolution3. External RAM: SRAM 8 MByteI have attached the project and vid...
I am trying to run a USB HS example with external PHY on NUCLEO-F756ZG. As I count find example I have gone ahead and created code from scratch. I am using USB3300 external PHY. I have made the proper connection except for RST and +5V to the module b...