User Activity

Hello,I am currently working on a project using the STM32 series and have two specific questions regarding MCU selection::keycap_1: Are there any STM32 MCUs that support 5V logic levels for both input and output?Most STM32 MCUs operate at 3.3V logic ...
Hello,I am currently working on sensorless PI control for a BLDC motor, and I am using the STM32F303ZE MCU for this project.In sensorless BLDC motor control, the motor must transition to the next commutation step 30 electrical degrees after the zero-...
Kudos given to