User Activity

Good day everyone. I am working on the STM32H7 MCU and using the HAL library for controlling an SPI in DMA mode that has to exchange data with an external device in real-time. I'm working at the maximum possible CPU frequency and using the -O2 optimi...
I am working on a STM32H723 microcontroller and I am trying to use and SPI communication in mixed mode, i.e. normal and DMA.The reason I need this is because I have a third party software stack for a device that is set up in a certain way, and it cyc...
I am using the Nucleo-STM32H723ZG board and I'm trying to set up a maximally reactive UDP/TCP communication channel between the board and an external node.Just to use a common ground, lets take as an example project the LwIP_UDP_EchoServer. If I send...
Kudos from
Kudos given to