STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L471 ADC maximum sampling rate

I have the following clock tree for STM32L471I am using TIM2 as trigger for DAC, ADC1, and ADC2 at 2.4MHz. Clock frequency of TIM2 is 48MHz with a counter value of 19 and prescaler = 0.With oscilloscope, I confirmed that the DAC is generating the sig...

kasarghu_0-1751879106670.png
kasarghu by Associate
  • 1053 Views
  • 3 replies
  • 2 kudos

STM32G491 MCU Power Delivery Specification

Hi STM Team,  We are planning to use STM32G491 MCU in our application. As per datasheet, it is mentioned that STM32G491 MCU will support USB PD 3.0. We have come across the below STM document where it is mentioned that "STM32 UCPD MCUs are compliant ...

MB.13 by Associate II
  • 1061 Views
  • 5 replies
  • 0 kudos

STM32H7 Enabling and disabling FMC

Hello,I'm using a specific board where the STM32 cohabit with another "master" device on the parralel bus.One time the STM32 is the master and "drive" the external RAM and one time the other device "drive" this RAM.My first thought was to disable the...

Alex_J by Associate II
  • 699 Views
  • 2 replies
  • 0 kudos

Resolved! SPi communication in stm32f407vgtx board

Hi allI am working with SPI1 on stm32f407vgtx and issue what I am, facing my NSS which internally controlled by SPI is taking more time for goes high even CLOCk has been stopped . my configuration are SPI full duplex 16 bit data clock is 2.6MHZ after...

Ash1_0-1752577116863.png
Ash1 by Associate III
  • 1880 Views
  • 14 replies
  • 5 kudos

Resolved! Stm32L443 stable code loading problem

 I’m using the STM32L443 in one of my products, and currently, there are around 2,500 units deployed in the field. I’ve been experiencing issues that I believe are related to the firmware programming process during production. The product includes a ...