STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MEM_MODE resets to 0x00 e v e r y t i m e (stm32f072)

I want to move the isr vector table to SRAMRelated to this questionI moved my isr vector table to SRAM (linker script)Now i want to aliase the memory addr of 0x0000 0000 to be found in SRAM.In order to do that i believe i need to change the bits from...

0693W00000BblMRQAZ.png
Javier1 by Principal
  • 1319 Views
  • 1 replies
  • 0 kudos

Hi, I am using STM32H7A3 Nucleo Board. I am using HAL_UART_Transmit() to transmit UART data and HAL_UARTEx_ReceiveToIdle_DMA() for receiving data.

Is  the below calls are required between every transmit and receive call, if we are using DMA? if(HAL_UART_DeInit(&UartHandle) != HAL_OK) {  Error_Handler(); }   if(HAL_UART_Init(&UartHandle) != HAL_OK) {  Error_Handler(); }Please give a clarificat...

JJoy.1 by Associate III
  • 2472 Views
  • 4 replies
  • 0 kudos

Resolved! Trying to make a Queue module for multiple UARTs

Hi gang. My application uses from 0 to 3 UARTs, or maybe USB CDC instead ... LOTS of end-user settable options. Even before I get to that, I'm not happy with my queue implementation that's to be used with UART (or CDC) Tx and Rx. I would love for th...

Grant Bt by Senior II
  • 3807 Views
  • 6 replies
  • 1 kudos

Why SPI returns busy after a while of sending correctly?

Hello ST community,I use a STM32F767ZI-Nucleo. There is a timer generating interrupts every 20ms. If a timer interrupt occurs I use HAL_SPI_Transmit_DMA to send some data. I monitor the return value of this function and after some time of sending wit...

LBaum.3 by Associate II
  • 22026 Views
  • 12 replies
  • 0 kudos