User Activity

HI ,I am new to the STM controllers and STM32Cube IDE.While loading the code i can see the only some sectors (i.e from 0 to 30 sectors or 0 to 64 sectors) are erasing and loading the new program...Please suggest me how to erase the complete interna...
Hi , i am new to some of the peripherals of STM32 controllers...I am using STM32L151RCT6 MCU in STMCube IDE for my application..My requirement is like i need to receive the new firmware binary file via Y modem and need to write into the flash and nee...
I am working on STM32L151RCT6 controller in STMcube IDE.. i have one application running in the Flash from starting address and one more application i want to run it from other location of Flash..basically 2 block of firmware(applications) i am consi...
Hi ,I not used RTC earlier and new to RTC.I am using STM32L151RCT6 MCU and creating the project in STM32Cube IDE.what are the settings i need to do to get RTC timing of 12 sec..I searched and got some information about alarm time setting and alarm in...
HI ,I am using STM32L151RCT6 MCU and creating the project using STM32Cube IDE..My requirement is like- need to calculate the average of some samples in particular time period that is 12 sec timing using RTC- ( it is like Moving average filter calcu...
Kudos from