STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Please someone help me in finding the datasheet for STM32F072RB in order to look into the "Alternate function mapping" of the GPIO pins.

I am using STM32F072RB Nucleo board and in the technical reference manual it is mentioned that "Please refer to the “Alternate function mapping�? table in the device datasheet for the detailed mapping of the alternate function I/O pins.". But I am no...

HD.1 by Associate
  • 1355 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F030C8 GPIO Max Source Current is limited to <5mA

Device Used : STM32F030C8, 48pin LQFP48I am driving MOC3043 Opto-Isolated Triac Driver so I need atleast 5 mA current sourced from the GPIO outputGPIO used with the MOC3043 is PA15 max current observed is 4.86mAOnly a single GPIO is configured at a t...

NFern.1 by Associate III
  • 4786 Views
  • 4 replies
  • 0 kudos

Adc using DMA for sine wave

Hi,​ Iam using DMA technique to digitise a sine wave using nucleo-H743ZI2, where Adc clock frequency is 36.5MHZ . Iam taking single data at a time and sending out using usart with a baud rate of 250000, the issue I am facing is when I increase th...

GHARI.1 by Associate II
  • 5556 Views
  • 12 replies
  • 0 kudos

How to debug both cores of the STM32H745 simultaneously?

Hello!i am working with the stm32h745 nucleo 144 board.i want to be able to debug both cores simultaneously using the onboard STLINK debugger, with no luck so far.followed the instructions from this ST document: https://www.st.com/resource/en/applica...

yuri CH by Senior
  • 1422 Views
  • 2 replies
  • 0 kudos

How should I build an effective peripheral "driver" ?

I've spent a fair amount of time getting small bits of code working so I can build them up into a larger working application. The code below works but I'm struggling with a way to move the parts related to GPS and the UART into separate files or clas...

magene by Senior II
  • 1127 Views
  • 1 replies
  • 0 kudos

Bipolar output from stm32g4 DAC.

Hello, I want to use external audio op amp, OPA1622 of TI. As in the attached photo, this opamp works using bipolar input. So, please guide me how is that possible using the output of STM32G4 DAC. Regards.

Sgupt.1 by Associate
  • 2269 Views
  • 2 replies
  • 0 kudos

Optimizing wake up time STM32L0.

I am trying to get an STM32L0 MCU to startup as quickly as possible. The datasheet says 5us wake up time from flash memory, but I am getting nowhere close to this. I loaded a super simple program that just toggles a GPIO and watched it on a logic ana...

TAnde.6 by Associate II
  • 3453 Views
  • 6 replies
  • 0 kudos