STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO Analog Mode vs Alternate Function ADC

Hello,I am trying to do a voltage measurement, i know i can use ADC to do it. What a gpio is capable of when it is configured as Analog Mode? Can it measure voltages? or Can it trigger an interrupt if a defined threshold exceeds?I need a clarificatio...

How to clear the SPI RX FIFO (register mode)

Hi all, I have an issue. I need to see the Slaves free space, for that, I am reading the slave's Empty space, and based on the results I send the data points which needed. but I am having a big issue. it always has a one execution cycle delay. For ex...

Roshan by Associate III
  • 4030 Views
  • 4 replies
  • 0 kudos

BlueNRG_LP multiple channel ADC

I am working with BlueNRG LP.I am acquiring 3 channels:ADC_VINP0 (PB3)ADC_VINM0 (PB2)BATTERY.I used and modified example of the "BlueNRG-LP Navigator" ADC_DMA.I read ADC_VINP0 and the batteries but ADC_VINM0 not work!! ( I used STEVAL-IDB011V1 and i ...

Hi im working on stm32l072cbt6 micro controller im trying to read the adc value on channel1 in polling method i generated the code using stm32 cube ide,the issue is that always i could not se any variation in the adc raw values and my code is as below,

void MX_ADC_Init(void) {   /* USER CODE BEGIN ADC_Init 0 */   /* USER CODE END ADC_Init 0 */   ADC_ChannelConfTypeDef sConfig = {0};   /* USER CODE BEGIN ADC_Init 1 */   /* USER CODE END ADC_Init 1 */ /** Configure the global features of ...

NJP.1 by Associate III
  • 2262 Views
  • 6 replies
  • 0 kudos

Resolved! STM32F107 I2C1 & I2C2

Hello,I am going to replace STM32F107 instead of F105 in my design, and as I see F107 has only one serial interface I2C1. In my case, I need both I2C1 and I2C2. Is there any way I can remap or define some pins as I2C2?Thank you.

NASI by Senior
  • 1465 Views
  • 2 replies
  • 0 kudos

How to calibrate ( RTC )LSE Crystal by temperature ?

I ' ve been working on a device that able to use industrial area. I must be sure that rtc clock is accurate because this device need to use RTC too much. When i researched , i did not find any code example about rtc calibration by temperature. Any su...

oziesin by Associate III
  • 3918 Views
  • 5 replies
  • 0 kudos

Resolved! STM32U585QI SPI Issue

Hi,I have successfully configured the SPI1 with following parameters and trying to transfer a single byte but it is being timed-out in HAL_SPI_Transmit as EOT is not being set.Init.Mode = SPI_MODE_MASTER;Init.Direction = SPI_DIRECTION_2LINES;Init.Dat...

Ramin1 by Associate II
  • 2582 Views
  • 3 replies
  • 0 kudos