STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SNMP Agent implemention

Hello,I want to implement the SNMP agent based on standalone, not based on os.I could have got a example code for snmp agent?Thank.

Kim.Andy by Associate III
  • 4036 Views
  • 1 replies
  • 0 kudos

Resolved! Which manual/reference contains detailed register/function specification for (USART) peripherals found in STM32F0 series?

I need to configure one of the USART peripherals in STM32F0 series MCU without using HAL or Low-layer drivers. I plan to fully initialize and drive the USART peripheral registers directly from the application, including assigning the USART to the req...

0693W00000JN8usQAD.png
wb0gaz by Senior
  • 1145 Views
  • 2 replies
  • 0 kudos

Resolved! Character match on STM32F303K8

Hello,I'm trying to set up the character match interrupt to detect the character '\n' (which indicates the end of a packet) and I don't manage to get the interruption.The procedure I'm using is:initialize the uart, its gpios, and the dma.enable the u...

Synchronized PWM outputs with offset?

Is it possible in the STM32 world to have two synchronized PWM - but with an offset separating the outputs?Here's the problem in picture form:Both the blue and red traces are the same frequency and duty cycle, but in this case trace red is offset 50 ...

0693W00000JMwz7QAD.png
DPaul.2 by Associate II
  • 4401 Views
  • 4 replies
  • 0 kudos

Resolved! Does STM32H743 Errata 2.16.2 apply to revision V silicon?

STM32H743Does errata 2.16.2 "Wrong data may be read from Message RAM by the CPUwhen using two FDCANs" apply to silicon revision V?The errata indicates it does, but previous discussion by Imen Dahmen indicates the issue was corrected. I need a confirm...

MBC by Associate III
  • 1804 Views
  • 2 replies
  • 1 kudos