cancel
Showing results for 
Search instead for 
Did you mean: 

İF İ ADD İWDT to my project İN CUBE MX v4.26.0 --L6200E

TARHAN SAMAH
Senior

HELLO ive created a project in cubemx v4.22. later i changed to new version i mean i downloaded the v 4.24.0 if i add iwdt then i get the project it doesnt compile ,

igot this error

compiling system_stm32f1xx.c...

linking...

ROVER_LORA\ROVER_LORA.axf: Error: L6200E: Symbol SystemCoreClock multiply defined (by system_stm32f1xx_1.o and system_stm32f1xx.o).

ROVER_LORA\ROVER_LORA.axf: Error: L6200E: Symbol AHBPrescTable multiply defined (by system_stm32f1xx_1.o and system_stm32f1xx.o).

ROVER_LORA\ROVER_LORA.axf: Error: L6200E: Symbol APBPrescTable multiply defined (by system_stm32f1xx_1.o and system_stm32f1xx.o).

ROVER_LORA\ROVER_LORA.axf: Error: L6200E: Symbol SystemInit multiply defined (by system_stm32f1xx_1.o and system_stm32f1xx.o).

ROVER_LORA\ROVER_LORA.axf: Error: L6200E: Symbol __asm___18_system_stm32f1xx_c_5d646a67____REV16 multiply defined (by system_stm32f1xx_1.o and system_stm32f1xx.o).

ROVER_LORA\ROVER_LORA.axf: Error: L6200E: Symbol __asm___18_system_stm32f1xx_c_5d646a67____REVSH multiply defined (by system_stm32f1xx_1.o and system_stm32f1xx.o).

ROVER_LORA\ROVER_LORA.axf: Error: L6200E: Symbol __asm___18_system_stm32f1xx_c_5d646a67____RRX multiply defined (by system_stm32f1xx_1.o and system_stm32f1xx.o).

ROVER_LORA\ROVER_LORA.axf: Error: L6200E: Symbol SystemCoreClockUpdate multiply defined (by system_stm32f1xx_1.o and system_stm32f1xx.o).

Not enough information to list image symbols.

Not enough information to list the image map.

Finished: 2 information, 0 warning and 8 error messages.

"ROVER_LORA\ROVER_LORA.axf" - 8 Error(s), 1 Warning(s).

what is wrong , what should i do ?? help needed

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

>>what is wrong , what should i do ?? help needed

You have two different copies of the system_stm32f*.c files in your project, remove ONE

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TARHAN SAMAH
Senior

THANKS

sureshsupriiiiii
Associate

linking...

Error: L6200E: Symbol SystemInit multiply defined (by system_stm32l4xx_1.o and system_stm32l4xx.o).

Error: L6200E: Symbol __asm___18_system_stm32l4xx_c_5d646a67____REV16 multiply defined (by system_stm32l4xx_1.o and system_stm32l4xx.o).

Error: L6200E: Symbol __asm___18_system_stm32l4xx_c_5d646a67____REVSH multiply defined (by system_stm32l4xx_1.o and system_stm32l4xx.o).

Error: L6200E: Symbol __asm___18_system_stm32l4xx_c_5d646a67____RRX multiply defined (by system_stm32l4xx_1.o and system_stm32l4xx.o).

Error: L6200E: Symbol AHBPrescTable multiply defined (by system_stm32l4xx_1.o and system_stm32l4xx.o).

Error: L6200E: Symbol APBPrescTable multiply defined (by system_stm32l4xx_1.o and system_stm32l4xx.o).

Error: L6200E: Symbol MSIRangeTable multiply defined (by system_stm32l4xx_1.o and system_stm32l4xx.o).

Error: L6200E: Symbol SystemCoreClock multiply defined (by system_stm32l4xx_1.o and system_stm32l4xx.o).

Error: L6200E: Symbol SystemCoreClockUpdate multiply defined (by system_stm32l4xx_1.o and system_stm32l4xx.o).

Not enough information to list image symbols.

I have also same problem..I got these errors after code generation through stm32cubemx . I have changed the Stm32cubemx version. That is iam getting this errors. i can solve this using previous version but i want to keep my code portable to any upcoming versions.

Did you get an answer to your problem, I am having the same issue.