Skip to main content
Linas L
Senior
August 18, 2021
Question

STM32 UART boot-loader Go command is unclear AN3155

  • August 18, 2021
  • 2 replies
  • 798 views

Hello,

I am implemented UART bootloader on my windows controlled test bench. All is great and working, but some uncertain exist with jump command.

Its says in app note:

jumps to the memory location programmed in the received ‘address + 4’ 
(corresponding to the address of the application reset handler).
For example if the received address is 0x0800 0000, the bootloader jumps to the 
memory location programmed at address 0x0800 0004.
In general, the host must send the base address where the application to jump to is 
programmed.

My understanding is that my program starts at 0x0800 0000. So I should jump to 0x0800000-4 ?

If I do so, I get NACK, and nothing happens. But if I jump to 0x0800000, all it's good. My program seems to be running, but based on application note, it means I am jumping to 0x08000004 address

So what is in that first 4 bytes of data at the start of the flash It says reset handler, so I suppose to jump over this point ? So this is why I am jumping just a bit further into flash, since bootloader already does this for me ?

In app note:
-> initializes the main stack pointer of the user application

Any insight will be welcome !

    This topic has been closed for replies.

    2 replies

    TDK
    August 23, 2021

    The first thing in your program is the ISR vectors. The first entry is used to store the end of the stack (_estack) which gets loaded into the MSP register. The second entry is the Reset_Handler pointer which is the entry point for your application.

    You should be sending 0x08000000 to the GO command.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    Tesla DeLorean
    Guru
    August 24, 2021

    Not actually "jumping" to the address you give it, but SP/PC pair pointing indirectly at other things.

    Data is a table, not executable code.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..