STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Two leds based on one interrupt line

Dear sir,I am using STM32F769NI microcontroller. I want to glow to different Leds on one external interrupt line i.e. Led1 on rising edge and Led2 on falling edge. Can you please suggest me the solution.Regards,Manoj

LL_TIM counter seems not actually counting.

I have this code: //SystemCoreClock=64 MHZ LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM6);  LL_TIM_SetPrescaler(TIM6, __LL_TIM_CALC_PSC(SystemCoreClock, 1000)); /* 1 tick /1 ms */LL_TIM_EnableCounter(TIM6);time0 = LL_TIM_GetCounter(TIM6);LL_mDela...

PTsou.1 by Associate
  • 1459 Views
  • 1 replies
  • 0 kudos

STM32H755 HAL_MMC_GetCardCSD() bug report.

Environment:tool: STM32CubeMX6.4.0 cpu: STM32H755XIRepos: STM32Cube_FW_H7_V1.9.1​The following lines in HAL_MMC_GetCardCSD() is probably incorrect.​ pCSD->EraseGrSize = (uint8_t)((hmmc->CSD[2] & 0x00004000U) >> 14U);​ pCSD->EraseGrMul = (uint8_t)((...

0693W00000KaP4PQAV.png 0693W00000KaP4ZQAV.png
Lzhou.1 by Associate
  • 730 Views
  • 0 replies
  • 0 kudos

Resolved! Encoder/Decoder Adat protocol on STM32 MCUs

Hello everyone.I need to implement a encoder/decoder for ADAT protocol (see https://ackspace.nl/wiki/ADAT_project for more details about ADAT protocol) and I don't know if some STM32 MCUs is able for that.As you can see in the image the encoder must...

0693W00000KaEixQAF.png
Arubu by Associate II
  • 5384 Views
  • 9 replies
  • 0 kudos

STM32l4 doesn't quit STOP2 mode if not debugging

Hello STM32-Community,right before finishing work and everything working arguably fine, I was trying to measure the power consumption of my periphery, where I could see that the program stopped working. I've pinned down the problem to not reentering ...

crackl1ng by Associate III
  • 1141 Views
  • 1 replies
  • 0 kudos

Is it normal to have to manually press the reset button on the development boards to connect to the development boards?

Hi! I am grad student that is a newcomer to the STM32 MCU platform. I want to ask a question about the problems I have been experiencing with my development boards. Is it normal to have to manually press the reset button on the development boards to ...

0693W00000KaCn7QAF.png 0693W00000KaCnMQAV.png 0693W00000KaCoFQAV.png
jhin by Associate II
  • 4123 Views
  • 5 replies
  • 1 kudos