STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BACKUP SRAM affects the other tasks

Hi,I am using backup sram in stm32f429zi. Data Read write in backup sram section is executing properly and data will retain after power down. But when we do the power UP then my program is not executing from main loop. so my code is not working as re...

ADank.2 by Associate II
  • 1794 Views
  • 2 replies
  • 0 kudos

stm32l476 a/d questions

If I am doing software trigger single conversion of 3 a/d channels and I set my end of conversion selection to be 'End of Single conversion' (CubeMX): Can I expect my to enter my ISR A/D callback at EACH EOCIF?All indications are that if I read the A...

SWenn.1 by Senior III
  • 874 Views
  • 1 replies
  • 0 kudos

STM32-HAL CAN transmits empty messages

I'm trying to transmit messages through CAN using HAL library. For test I repeated code from the first part of this video I have the same bluepill so I just did the same. Also I've tried his project, but changing Nucleo RE to ZE model. I've looked th...

0693W00000KaJJxQAN.png 0693W00000KaJKbQAN.png
LFili.2 by Associate
  • 1163 Views
  • 0 replies
  • 0 kudos

SPI Slave mode using DMA and soft NSS

I'm trying to transmit some data using DMA as a slave SPI device. I'm sending 8 byte but the peripheral always gives me 9 byte on the MISO line (first byte twice). The Master NSS is connected to a GPIO input (SPI_ENABLE) using external interrupt Mode...

0693W00000JOrukQAD.jpg
wh by Associate III
  • 6197 Views
  • 5 replies
  • 0 kudos

Please improve DFSDM section of reference manual.

I've managed to get the DFSDM working with a PDM microphone (on a STM32L496 board) - using direct access to registers. But the documentation often made things more difficult than they needed to be. Just a few extra sentences, less ambiguous language ...

gregstm by Senior III
  • 4126 Views
  • 9 replies
  • 1 kudos

How to switch the operator for B-L462E-CELL1 board?

Hello,I wanted to experience data transmission through NB-IoT in Canada by using a Cellular Discovery Kit (B-L462E-CELL1).The eSIM is activated and the board communicates with echoclient, but it selects the operator automatically. Unfortunately, the ...

S.R.M. by Associate
  • 608 Views
  • 0 replies
  • 0 kudos

Effect of pull up without supplying power to MCU

As shown in above figure.The EXT/GPIO pin directly connected to MCU with pull up resistor (10K).So once the switch press the PMOSFET start switching supply to MCU.Please let me know the effect of voltage on EXT/GPIO pin without suppling power to MCU.

0693W00000KaBiuQAF.png
cWagh.1 by Associate
  • 1656 Views
  • 4 replies
  • 0 kudos