STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

sample rate using DMA, ADC and Timer

Hi, I need to sample a signal at a frequency of 10kHz. To avoid the use of the microprocessor I thought of doing it using a 10kHz Timer that triggers the ADC conversion on its falling edge, in addition, I need the ADC read value to be transferred via...

LSoll.1 by Associate II
  • 4394 Views
  • 7 replies
  • 0 kudos

Resolved! offset on the ADC

I want to read the Vdd (link to VDDA) of my board with the ADC in a STM32L072. I try read it through a divider bridge or through VrefInt, and both give me a value far below the voltmeter value.here is my config: hadc.Instance = ADC1; hadc.Init.Ov...

Ppeyr.1 by Associate III
  • 6363 Views
  • 9 replies
  • 0 kudos

CAN TX stopped working

Hello, I'm using stm32F446RE.Sending CAN messages to two controllers and it stopped working after some seconds if time delay between the messages is less than one second, And it's slow for my project.looking for suggestions, attaching some of my code...

SPati.9 by Associate II
  • 737 Views
  • 0 replies
  • 0 kudos

Resolved! Clear Tim1 --- STM32L476RG?

Hello All....Simple question. I am using the functions(HAL_TIM_Base_Stop_IT and HAL_TIM_Base_Start_IT). Basically I set a timer to count to a value and an interrupt occurs. The timer starts on a GPIO edge. I would like the timer to always zero out at...

SWenn.1 by Senior III
  • 1408 Views
  • 2 replies
  • 0 kudos

RTC Internal timestamp is only updated when the first time RTC is initialized and power shifted to VBAT. On further power up and shutdown events that RTC Timestamp registers are not being updated with new time stamp values.

 I'm reading TS and clearing TSF, ITSF, TSOVF flags upon power up. But when power cycle happens again, the TS registers are still containing the previous value, but not present value.

vamsi by Associate II
  • 1612 Views
  • 3 replies
  • 0 kudos

Resolved! 32bit input capture (AN2592) inaccuracy

Apnote "Achieving 32-bit timer resolution with software expansion" (AN2592) mentions that it is possibleto create 32bit input capture with only one 16bit timer. Combine interrupt from update event to count timer overflows and regular 16bit input cap...