STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN protocol forwarding limits?

Hi, I would like to forward about 2048 bytes via CAN protocol.I am using an STML4 and have implemented a solution in which sending an STM transmits in the following way:void CAN1_Tx(){ CAN_TxHeaderTypeDef TxHeader; uint32_t TxMailbox; uint8_t message...

JTLGE by Associate II
  • 1124 Views
  • 2 replies
  • 0 kudos

Multiple I2C DMA requests on STM32H7, chained together

Hi, I want to transmit the following sequence with DMA, ideally without any interrupt (except once all the data transferred i.e. at the end of the whole operation).I'm talking in I2C with a device that works like that :Send one byte for read request ...

YB.1 by Associate
  • 2101 Views
  • 2 replies
  • 0 kudos

GPIO output voltage level in stm32g4

I want to know the ouput level of the pin PA3 wich has a structure as TT_a (3.6 V tolerant I/O)the table provided in the datasheet is a bit tricky to understand. Which are the row that I should consider for the PA3 pin? Cmos or TTL or the others?

0693W00000LwX6qQAF.png 0693W00000LwX75QAF.png
Tommino by Senior
  • 2274 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H725 NVIC priority and subprioririty

Hi!I try to set IRQ priority to 3 and subpriority to 2.HAL_NVIC_SetPriority(EXTI9_5_IRQn, 3, 2);I suppose that correspond NVIC IPR [23] now is 0x32. But it is 0x30. I read AIRCR PRIGROUP (it is 3).uint32_t PriorityGroup = NVIC_GetPriorityGrouping();A...

Aleks by Associate III
  • 4676 Views
  • 2 replies
  • 0 kudos

I need to send 2 bytes over the I²c bus with a STM32L432 as slave and a Raspberry Pi as master. But the clockpulse of the SCL is to wide.

In the code below I send 2 bytes with my STM32 (I've chosen a number higher then 255 (340) so it needs to send the data in 2 bytes) but on the scope I cant find this data. I guess it's because of the wide clockpulse and the Rpi expect an ACK. Instead...

0693W00000LwSUdQAN.jpg 0693W00000LwSUTQA3.jpg 0693W00000LwSUOQA3.png
WFouq.1 by Associate II
  • 1881 Views
  • 1 replies
  • 0 kudos

Using flash algorithm from F103 for F405

Hi,I am trying to use a flash write and read module written for the STM32F103 on an STM32F405.However the F103 deals with pages and subpages. Some algorithms depend on subpage size. The F405 has sectors, which I guess are the equivalent to pages, but...