2021-11-04 3:36 AM
stm32f207zg (nucleo-f207zg)
Hi, im trying to write into my DMA2 Stream0 CR register (mapped as 0x40026410).
But that memory addr cannot be written not with my init code nor manually trough the STM32IDE debugging tools .
Is there any memory protection or lock i am missing?
Solved! Go to Solution.
2021-11-04 3:42 AM
Hello @Javier Muñoz
Just a basic question: Did you enable the DMA2 clock ? (RCC_AHB1ENR bit 22) ?
(or call corresponding HAL/LL to do it)
BR,
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-11-04 3:42 AM
Hello @Javier Muñoz
Just a basic question: Did you enable the DMA2 clock ? (RCC_AHB1ENR bit 22) ?
(or call corresponding HAL/LL to do it)
BR,
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-11-04 3:53 AM
Howdy @Bruno_ST
Ding ding ding!, that was it.
Im using autogenerated CUBEMX code.
It looks like CubeMX places ADCDMA config after the DMA clock is enabled (RCC->AHB1ENR), so thats why it wasnt working
If i move the MX_DMA_Init before the ADC init everything works