User Activity

STM32g474 code execute automatically without pressing RUN when i put MCU in debugging mode in uVision.Anyone knows where im wrong?Note:- Reset pin is not connected pull up or down.
I m working with STM32 MCU from last 3 years  i made many boards for STM MCU but i never face the problem which I'm facing now. In past i made boards for lower pin packages ( up to LQFP 64 ) mostly they have single power input pins this time i made a...
I have almost 2 year experience with stm32 MCU. if I had any problem I solve it with in one or two days. But right now I'm facing a very strange problem and stuck on it from last 25 days.. I'm working on Grid connected inverter control board. In desi...
/* USER CODE BEGIN Header *//** ****************************************************************************** * @file      : main.c * @brief     : Main program body ****************************************************************************** * @at...
Kudos given to