STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Memory leak detection or profilers

I am using STM32CubeIDE suite of tools on windows. MCU is STM32F4. Debugger is ST-Link V2.Is there a way to identify memory leak in the code i wrote for my MCU ? Preferably in STM32CubeIDE as its through this tool I upload & debug firmware for MCU.I ...

MSing.8 by Associate III
  • 6010 Views
  • 5 replies
  • 0 kudos

STM32H743VIT6. FMC for SDRAM

Hi,Is SDRAM over FMC supported in STM32H743VIT6 MCUs? I can't see this option in CubeMX, only NOR Flash/PSRAM/SRAM/ROM/LCD and NAND Flash. The datasheet says that SDRAM is not supported in LQFP144 packages, but my one is LQFP100.Looking forward for a...

OIrin.1 by Associate II
  • 2439 Views
  • 4 replies
  • 0 kudos

How do you specify GPIO ports and pins as function inputs?

I am new to STM32s programing in general and am trying to create some simple libraries, altough I have no idea how I would make it so that I can write it in a way, that needed ports and pins are given in function inputs. For example: int HCSR04_Dista...

LTork.1 by Associate
  • 2355 Views
  • 2 replies
  • 0 kudos

Resolved! Send .bin file through UART

Hello, i am using a STM32L0xx series, i just finished my bootloader than can init and jump an application from the specific location in Flash memory, so the only thing left to do is getting bin file (data) from the usart, but how can i send a .bin fi...

RComa.1 by Associate II
  • 7556 Views
  • 4 replies
  • 0 kudos

Resolved! How do you implement an I2C Slave to look like a memory?

Here is what I am trying to Implement. To make the I2C Slave look like a memory to the master. Syntax is one of two cases. For a Write:<Dev Add W><MemAdd MSB><MemAdd LSB><Data0><Data1>...<Data N><Stop>For a Read:<Dev Add W><MemAdd MSB><MemAdd LSB><Re...

KiptonM by Lead
  • 7004 Views
  • 9 replies
  • 0 kudos