STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Resetting the IWDG on wakeup using HAL STM32L011K4T

Hi all,I believe I am having a problem with the IWDG in my project. What's happening is that immediately after entering sleep mode the device wakes up again.From the research I have done, it looks like this is inevitable, and in order to deal with it...

LMill.2 by Associate
  • 1875 Views
  • 2 replies
  • 0 kudos

STM32L071 Multiple channels ADC using DMA

Hey. I am trying to read multiple ADC channels using DMA but with no luck. My project settings:I have selected 4 channels and enabled Continuous conversion mode as well as DMA Continuous requests. I have also created a circular DMA for ADC : #include...

0693W00000LyK4lQAF.png 0693W00000LyK50QAF.png 0693W00000LyK5yQAF.png
LPetr.1 by Senior II
  • 2240 Views
  • 4 replies
  • 0 kudos

Compute cpu load for a STM32L0, a gpio and a voltmeter

Hello,At work we have developed firmware on a stm32l0 based on different time base with systick and counters of elapsed time (10ms, 100ms and 1s). Therefore, some function are executed periodically.The board is powered with 3.3V.In order to measure c...

SLE G.1 by Associate
  • 5354 Views
  • 7 replies
  • 0 kudos

Resolved! HAL_RTC_GetTime return 1 instead of 13

Hello ST community! We're using STM32F401RDT6.We use the RTC to maintain scheduled events that occur in the time we set, but not with the RTC's Alarm mechanism, rather our custom-made mechanism based on the current epoch time which is being updated e...

RLand.2 by Associate II
  • 2474 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.