User Activity

Hi ,For a GIVIEN Binary File . We Want to Implement STM32CUBEIDE Post Build CRC calculated Value to Match with the STM32 HW CRC value .For IAR WorkBench IDE the IDE Proviedes POST BUILD configuration to generate the required CRC and place in BINARY ....
We Want to Log Code Coverage Report for STM32H745XI Dual core CM7 and CM4 Controllers .With single Core Single Project the code coverage is not working we are using OZONE IDE and SEGGER PRO . We need help if SINGLE CORE CODE COVERAGE how ot trigger t...
Need support to have STM32F769 Hardware 32BIT CRC generation and same value should be generated by STM CUBE IDE POST COMPILATION 32BIT CRC for BINARY file .So a quick background is once the project is compiled and binary is generated we use SREC_CAT ...
After Completion of build with STM32CubeIDE in headless build mode,Is there an automated scrit that we can use STM32CubeProgrammer to program the binary to the STM32 board ?.
Is there any scripting support to STM32CubeIDE to load a project build the project and download the project using debugger to Microcontroller STM32H745XI
Kudos from