Hi guys,I'm currently working with Standard CAN. The maximum data length of each frame is 64 bytes. In HAL library, I see DLC parameter is limited from 0 to 8. So that means, I can only transmit 8 elements of an array (8 bytes for each element). In o...