STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC values are not stable in STM32H723ZG

Hello everyone,With respect to the Subject I am facing problem in reading analog voltage across the analog pins in the controller specified.Following are the ADC configuration.1. ADC resolution = 12Bit2. Sclk = 256MHz3. ADC clock source = Sclk/44...

Arrhenius by Associate III
  • 5229 Views
  • 5 replies
  • 0 kudos

H723ZG Nucleo ADC clock/noise question

After assembling the X3 external 25MHz crystal and 2 caps and generating initialize code for 550MHz clock with CubeMX my NUCLEO-H723ZG board runs fine, except ADC. It is very noisy. The CubeMX configured the clock for ADC = 96.000671 MHz (PLL2P). In ...

0693W00000Lwc7AQAR.bmp
Louie88 by Senior II
  • 7679 Views
  • 13 replies
  • 0 kudos

STM32L071RB RX Halt Issues

Hi, We have been experiencing severe issues with RX UART on STM32L071.The RX bus stops receiving data while running, and the only way we could recover from it was to initiate the UART back again which probably clears the registers.Is anyone familiar ...

Wich is the STM32F429 PLLN maximum frequency?

User' manual says that the maximum PLLN or VCO output frequency should be between 100 and 432 MHz (pg. 227). However, I was trying to set the PLL clock and the SysClock to 180 MHz and also respect the 48 MHz clocks.One possible solution is to set the...

TCabr.1 by Associate II
  • 6486 Views
  • 10 replies
  • 0 kudos

STM32L073 PC13 settings are affecting the LSE oscillation.

We are using STM32L073.When a 512Hz square wave is output to PC1 using LPTIM_OUT (source clock LSE), if the calibration output of PC13 is set to 512Hz, the PC1 output will make a large transition to about 509Hz at around -30 ° C. When set to NONE, th...

tsuna by Associate II
  • 1772 Views
  • 2 replies
  • 2 kudos

STM32F446 how to use rotary encoder with timer?

I have an application I am converting from another processor to a STM32F446 board. The application uses a rotary encoder to detect counts and direction.I have looked at several videos online on how to use a timer for rotary encoder purposes. I'm begi...

USART1 doesn't communicate using HSE; worked with HSI

Hello, I am new to the ST platform.I actually work with a nucleo144, and i was trying to work with bluetooth hc-06, the problem is that USART1 doesn't communicate with the board when I use HSE in the clock configuration, but it worked when I use HSII...

AAAZO.1 by Associate II
  • 1752 Views
  • 2 replies
  • 0 kudos