Skip to main content
RLosc.1
Associate II
July 22, 2020
Question

STM32F3 SPI3 not working

  • July 22, 2020
  • 5 replies
  • 2086 views

Hey,

I'm working with STM32F303RET6.

I'm having trouble transmitting data with SPI3 (PB3, PB4, PB5 and PA15).

Before I'll post my code here, I want to say that I am also working with SPI2 (PB12, PB13, PB14 and PB15) with the exact same configuration on MXCube and it works flawlessly.

I tried making everything simpler by creating a new project and only initializing the SPI3 and checking with the scope what's going on with SCK and MOSI but for some reason they stay idle.

I'm controlling NSS manualy because I had trouble with that before so at least the NSS is working correctly.

This is my simple MXCube generated code:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * <h2><center>&copy; Copyright (c) 2020 STMicroelectronics.
 * All rights reserved.</center></h2>
 *
 * This software component is licensed by ST under BSD 3-Clause license,
 * the "License"; You may not use this file except in compliance with the
 * License. You may obtain a copy of the License at:
 * opensource.org/licenses/BSD-3-Clause
 *
 ******************************************************************************
 */
/* USER CODE END Header */
 
/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
SPI_HandleTypeDef hspi3;
 
/* USER CODE BEGIN PV */
unsigned char Tx;
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SPI3_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 Tx = 0xB1;
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_SPI3_Init();
 /* USER CODE BEGIN 2 */
 HAL_GPIO_WritePin(SPI3_NSS_GPIO_Port, SPI3_NSS_Pin, GPIO_PIN_SET);
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
	 HAL_GPIO_WritePin(SPI3_NSS_GPIO_Port, SPI3_NSS_Pin, GPIO_PIN_RESET);
	 HAL_SPI_Transmit(&hspi3,&Tx,1,100);
	 HAL_GPIO_WritePin(SPI3_NSS_GPIO_Port, SPI3_NSS_Pin, GPIO_PIN_SET);
 
 }
 /* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief SPI3 Initialization Function
 * @param None
 * @retval None
 */
static void MX_SPI3_Init(void)
{
 
 /* USER CODE BEGIN SPI3_Init 0 */
 
 /* USER CODE END SPI3_Init 0 */
 
 /* USER CODE BEGIN SPI3_Init 1 */
 
 /* USER CODE END SPI3_Init 1 */
 /* SPI3 parameter configuration*/
 hspi3.Instance = SPI3;
 hspi3.Init.Mode = SPI_MODE_MASTER;
 hspi3.Init.Direction = SPI_DIRECTION_2LINES;
 hspi3.Init.DataSize = SPI_DATASIZE_4BIT;
 hspi3.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi3.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi3.Init.NSS = SPI_NSS_SOFT;
 hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
 hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi3.Init.CRCPolynomial = 7;
 hspi3.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
 hspi3.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
 if (HAL_SPI_Init(&hspi3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI3_Init 2 */
 
 /* USER CODE END SPI3_Init 2 */
 
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(SPI3_NSS_GPIO_Port, SPI3_NSS_Pin, GPIO_PIN_RESET);
 
 /*Configure GPIO pin : SPI3_NSS_Pin */
 GPIO_InitStruct.Pin = SPI3_NSS_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(SPI3_NSS_GPIO_Port, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 
 /* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{ 
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

What could be the source of the SPI3 not working??

Thanks in advance,

Rony.

This topic has been closed for replies.

5 replies

waclawek.jan
Super User
July 22, 2020

Read out and check/post the relevant SPI and GPIO registers content.

JW

RLosc.1
RLosc.1Author
Associate II
July 22, 2020
void HAL_MspInit(void)
{
 /* USER CODE BEGIN MspInit 0 */
 
 /* USER CODE END MspInit 0 */
 
 __HAL_RCC_SYSCFG_CLK_ENABLE();
 __HAL_RCC_PWR_CLK_ENABLE();
 
 /* System interrupt init*/
 
 /* USER CODE BEGIN MspInit 1 */
 
 /* USER CODE END MspInit 1 */
}
 
/**
* @brief SPI MSP Initialization
* This function configures the hardware resources used in this example
* @param hspi: SPI handle pointer
* @retval None
*/
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(hspi->Instance==SPI3)
 {
 /* USER CODE BEGIN SPI3_MspInit 0 */
 
 /* USER CODE END SPI3_MspInit 0 */
 /* Peripheral clock enable */
 __HAL_RCC_SPI3_CLK_ENABLE();
 
 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**SPI3 GPIO Configuration 
 PB3 ------> SPI3_SCK
 PB4 ------> SPI3_MISO
 PB5 ------> SPI3_MOSI 
 */
 GPIO_InitStruct.Pin = GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
 /* USER CODE BEGIN SPI3_MspInit 1 */
 
 /* USER CODE END SPI3_MspInit 1 */
 }
 
}
 
/**
* @brief SPI MSP De-Initialization
* This function freeze the hardware resources used in this example
* @param hspi: SPI handle pointer
* @retval None
*/

You mean this?

TDK
July 22, 2020

That code looks fine. Are you sure there's not a hardware error? If you initialize PB3, PB4, PB5 and PA15 as GPIO outputs, can you toggle them all and see them on the scope?

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
July 22, 2020

>You mean this?

No. I mean, read out what is actually in the registers.

Plus do what TDK said above.

JW

SCamp.1041
Associate III
March 8, 2022

Just want to jump in here as I had the same problem on an F446RE... I had to set `GPIO_InitStruct.Alternate = GPIO_AF6_SPI3`, apposed to `GPIO_AF5_SPI3` 🤷�?♂�?