2022-03-08 1:02 AM
Hi everyone, I'm trying to use the Timer2 CH2 PWM Mode 1 to generate a 1 Hz signal with 50% Duty Cycle out of my PA0 pin but i can't get anything. Here's my code:
#include"stm32f3xx.h"
void TIM_PWM(void);
int main(void){
TIM_PWM();
while(1){
}
}
void TIM_PWM(void){
RCC->AHBENR |= (1U<<17); //AHBENR GPIOA
RCC->APB1ENR |= (1U<<0); //APB1ENR TIM2
GPIOA->MODER |= (1U<<1); //PA0 alternate function
GPIOA->AFR[0] |= (1U<<0); //alternate function AF1 on PA0
TIM2->PSC = 8000;
TIM2->ARR = 1000;
TIM2->CNT = 0;
TIM2->CCR2 = 500; //capture compare CH2
TIM2->CCMR1 |= (0b110<<12); //capture compare PWM mode 1
TIM2->CCER |= (1U<<4); //capture compare CH2 output enable
TIM2->CR1 = (1U<<0); //counter enable
}I'm using a NUCLEO BOARD STM32F303RE. Clock is set to 8 Mhz.
Can someone help me? thanks in advance
Solved! Go to Solution.
2022-03-08 4:11 AM
> GPIOA->MODER |= (1U<<1); //PA0 alternate function
> TIM2->CCR2 = 500;
TIM2_CH2 is not on PA0 is, but TIM2_CH1 is.
Use CCR1 instead of CCR2.
Note that the period is (timer clock) / (PSC + 1) / (ARR + 1) so you don't quite have 50% duty cycle. Probably want PSC=7999, ARR=999, CCR1=500.
2022-03-08 4:11 AM
> GPIOA->MODER |= (1U<<1); //PA0 alternate function
> TIM2->CCR2 = 500;
TIM2_CH2 is not on PA0 is, but TIM2_CH1 is.
Use CCR1 instead of CCR2.
Note that the period is (timer clock) / (PSC + 1) / (ARR + 1) so you don't quite have 50% duty cycle. Probably want PSC=7999, ARR=999, CCR1=500.
2022-03-09 12:48 AM
I didn't notice that the CH was wrong. I fix the code and now it works as expected. Thank you very much!