STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer1 MOE and breakpoints

I am using an STM32F4 micro using TIM1_CH1 and CH2 outputs to create a communications signal with compare outputs. The first bit that I am outputting is wrong, so I would like so set a breakpoint to see what is going on. BUT, when I check the timer c...

gahelton1 by Associate III
  • 1192 Views
  • 1 replies
  • 0 kudos

Why measured pulse width using TIMER accumulates error as pulse width increases? (understanding inaccuracies in TIMER)

Dear All,Board: Nucleo - H745ZI-QWhat am I trying to do ?I am trying to measure pulse width of an signal using counter mode of timer 2, as accurately as possible. The input pulse width varies from 1 us to 1000 us.What have I done?I configure the Tim...

sarojj7 by Associate III
  • 2924 Views
  • 6 replies
  • 0 kudos

B-L475E-IOT01A Flash Erase & Write

I want to work on flash with B-L475E-IOT01A1.​After flash erase operation, flash write operation is performed, and memory is being checked through debugging.​On other boards, flash erase operation changed the memory in that location to the "?" mark, ...

GKIM.4 by Associate II
  • 717 Views
  • 0 replies
  • 0 kudos

Clock cycle behavior as a function of frequency

Hello, On the STM32F746ZG I measure the clock cycle needed to execute a code thanks to a timer which runs at the same frequency as the core clock.However, for the same code, with exactly the same measurements process, the clock cycle needed to execut...

TGA.1 by Associate
  • 2495 Views
  • 3 replies
  • 0 kudos

How is wrap-around handled in CCR registers

Apologize in advance for what may be a basic question. I have a background in C programming and other languages mostly at the application layer. I have however, supervised, reviewed, and analyzed embedded C code at lower layers from others. My curren...

RM0440, Rev 7, STM32G474 Reference Manual - Errors

Figure 188, Page 853: The last waveform (HRTIM_REPxR = 2) should be: 1, 0, 2, 1, 0 and not 1, 0, 2, 0.Figure 254, Page 933: For the last two waveforms (ADCxPSC[4:0]=4 ADROM[1:0]=01 and ADCxPSC[4:0]=4 ADROM[1:0]=10), it seems like the waveforms as sho...