STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G4 DMAMUX

Hello,Can you help me to use the DMAMUX in the STM32G474 microcontroller?How can I program the uC to make TIM2_CH1 sends a DMA request when CC. I have found this in the reference manual but I can't undesrtand which channel of the DMA is involved. Tha...

0693W00000LvzUZQAZ.png
Tommino by Senior
  • 7987 Views
  • 21 replies
  • 0 kudos

Measuring capacitance STM32L0-Disco

I'm trying to measure capacitance with my STM32L053-DiscoI'm using ADC and one output pin to charge the capacitor. I tried measuring time it takes for capacitor to charge to 62.3%.The problem that I'm facing is that the values that I'm getting from A...

0693W00000NpgdJQAR.png 0693W00000NpgdJQAR.png
JRubė.1 by Associate II
  • 5978 Views
  • 13 replies
  • 0 kudos

STM32G070 as the alternative to STM32G081

ST has confirmed that STM32G070 uses same silicon as STM32G081, thus we're considering use it as the alternative to STM32G081 due to availability problems.STM32G070 lacks BOR feature and CEC hw block acc. to datasheet but we have proven by trial that...

LPiro.1 by Associate II
  • 2929 Views
  • 4 replies
  • 1 kudos

spi in STM32H7

SPI in stm32h7 (stm32h743iitx in slave mode) don't work, receive wrong values.how I make spi to work correctly in stm32H7? its not clear at allthanks,

M4D by Associate II
  • 2898 Views
  • 6 replies
  • 0 kudos

Are there any errors associated with the CAN Controller on the STM32F205ZGT6 MCU which could explain the CAN bus packet failures when the ambient temperature is increased to 40°C?

Hi,I wonder if you can help us? In one of our projects we are using the STM32F205ZGT6 Microcontroller and specifically we are using the CAN bus. The problem is that when we increase the ambient temperature around the MCU to approximately 38°C to 40°C...

MColl.5 by Associate II
  • 2423 Views
  • 3 replies
  • 1 kudos

Resolved! STM32L011K4T6 Wake Up Pin Configuration

I've struggled with this for a few days and read a dozen forum posts that end unanswered.I am trying to put my micro controller into standby mode and then wake it up with an IMU pulling the PA0/SYS_WKUP1 pin high. What I am finding, which is somewhat...

LMill.2 by Associate
  • 5549 Views
  • 1 replies
  • 0 kudos

Resolved! WWDG_IRQHandler called after a blx instruction

Hi all,I'm trying to use a version of the elua interpreter on a stm32f446re nucleo board.I've encountered a problem, the program is jumping on an infinite loop after entering a couple of functions of the interpreter. The system is blocking in an WWDG...

NoeMurr by Associate II
  • 3013 Views
  • 3 replies
  • 0 kudos