cancel
Showing results for 
Search instead for 
Did you mean: 

Hello , I am uploading the code to the STM32H747 Discovery Kit board and it doesn't upload it although its writing that it does (log) I tried to erase the user flash memory, using pin R192, but it doesn't help , can you help with it.

EBarm.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @EBarm.1​, to the community!

If you put a resistor smaller than 3.2k or short-circuit R192, you will not delete the FLASH, but you will enter the bootloader after a reset (see AN2606, section 4 and 48).

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @EBarm.1​, to the community!

If you put a resistor smaller than 3.2k or short-circuit R192, you will not delete the FLASH, but you will enter the bootloader after a reset (see AN2606, section 4 and 48).

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.