STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can CM4 put CM7 core to sleep (or stop or halt)

I am using the template with CM7 as gated and CM4 core boot. This behavior works fine. In my application, CM4 runs on bank1 and CM7 runs on Bank 2. One sector on Bank 2 is dedicated to store application data. So CM4 tries to write to that sector, whi...

JTari.1 by Associate II
  • 993 Views
  • 0 replies
  • 0 kudos

TIM6 Interrupt and Compiler Optimization

I have a project (for STM32L0) that use TIM6 to generate an Interrupt every 5ms and everything works perfectly both in release and debug when built wih no optimization.Then I built the same project with -Os(optimize for Size) -ffunction-section -fdat...

MVill.6 by Associate II
  • 10599 Views
  • 10 replies
  • 0 kudos

Can I measure PWM duty cycle using DMA?

I am on STM32F401 and I want to measure PWM duty cycle (PWM input) with timer 3 and a DMA channel. I'd like to have the DMA to do several measurements and then calculate the average over it. My configuration is like this:My DMA config is like this:My...

0693W00000QKukTQAT.png 0693W00000QKukdQAD.png 0693W00000QKukiQAD.png
HStee.1 by Associate II
  • 4652 Views
  • 3 replies
  • 0 kudos

STM32 MODBUS

Im using nucleo stm32f103. Does a modbus library exist or how would one go on with using modbus? Could not find any tutorials online.

rtek by Associate II
  • 39402 Views
  • 7 replies
  • 0 kudos

WiSEStudio Build Analyzer

How to add Build Analyzer function in WiSEStudio IDE?Available on Atollic TrueSTUDIO IDE.​Thanks in advance.regards,fanyun.

fanyun by Associate II
  • 2236 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.