Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs products
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
STM32 MCUs Other solutions
STM32 MPUs
STM32 MPUs products
STM32 MPUs Boards and hardware tools
STM32 MPUs Software development tools
STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
Microcontrollers
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
HAli.2
Associate II
since
2022-02-09
2023-06-14
User statistics
4
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About HAli.2
Options
Report User
User Activity
Posts
Replies
i have STM32F103C8T6 suddenly the pins of the MCU is not working. Are the pins fried ? The 3.3v or 5v pins does not work when I connect a LED using 1k res. But when i try to run the Blinky app in eclipse and choose the internal LED PC13 to blink it works
2022-02-09
Re: i have STM32F103C8T6 suddenly the pins of the MCU is not working. Are the pins fried ? The 3.3v or 5v pins does not work when I connect a LED using 1k res. But when i try to run the Blinky app in eclipse and choose the internal LED PC13 to blink it works
2022-02-10
I used the GND of the st link programmer and tried all of GPIO pins and it worked.For some reason the GND of the MCU is not working.
Re: i have STM32F103C8T6 suddenly the pins of the MCU is not working. Are the pins fried ? The 3.3v or 5v pins does not work when I connect a LED using 1k res. But when i try to run the Blinky app in eclipse and choose the internal LED PC13 to blink it works
2022-02-10
The LED is working well and i already made sure of that. But with alot of testing i figured out that the problem is in the GND pins of the MCU somehow.
Re: i have STM32F103C8T6 suddenly the pins of the MCU is not working. Are the pins fried ? The 3.3v or 5v pins does not work when I connect a LED using 1k res. But when i try to run the Blinky app in eclipse and choose the internal LED PC13 to blink it works
2022-02-10
Well, I have already made sure of that. I connected an external 3.3v and it works well