STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-L073RZ, ADC reading problem on PA2 and PA3 pins We removed SB13 and SB14 resistors on NUCLEO-L073RZ board and configured PA2 and PA3 as ADC channels (in CubeMX), but AP2 and PA3 don't read any analogy inputs.

We also configured the other PAx pins, such as PA0, PA1, PA4, PA5, ect as ADC channels. these pins work properly.Removing SB13 and SB14 is based on the suggestion of NUCLEO-L073RZ manual (UM1724 Rev 14), in order to use PA2/3 pins.Please let us know ...

Texram by Associate III
  • 1711 Views
  • 4 replies
  • 0 kudos

Resolved! Query on SW compatibility between STM32L475RC and STM32L475RE

Hi,I have a project which is based on the STM32L475RC and now I want to upgrade to the STM32L475RE controller. I have changed the device from STM32L475RC to STM32L475RE in options for the target of the Keil environment. But the new project based on t...

Harish1 by Associate III
  • 2570 Views
  • 5 replies
  • 0 kudos

I want to use the WM8994 on the STM32F769-DISCO for 24 bit acquisition on the Line In connector. Unfortunately the BSP code is fixed at 16 bit. :-(

Has anyone done the changes necessary to switch up to 24/32 bit acquisition. It seems like its just AIF1_Control[6,5] on the WM8994 but the SAI is a complex beast and I'm not having a lot of luck. Any pointers would be greatly appreciated.

IWhit.2 by Associate II
  • 793 Views
  • 0 replies
  • 0 kudos

DMA HALFWORD and SAI_DATASIZE_24;

Posted on June 29, 2018 at 07:30Hi, I'm trying to use SAI_DATASIZE_24; with the Audio_playback_and_record application demo for the STM32f769i_Discovery.The demo uses DMA to copy data from the SAIx to the recorder buffer in 16bit.I tried changing the...

benyBoy by Associate II
  • 3093 Views
  • 4 replies
  • 0 kudos

Resolved! Does STM32U5 series supports 1us hardware timer ?

I am looking for maximum timer resolution supported in STM32U5 series MCU's.Basically whether I can configure or use hardware timer as 100us.Any input or documentation on this would be a great help.Thanks!!

NM.1 by Associate II
  • 1916 Views
  • 3 replies
  • 0 kudos

Getting elapsed time after stop mode

Hello,I am looking for help. I am using stm32L0. The problem is as follows:ST goes in stop mode for example 5 seconds. After 2 second some interrupt wakes the ST. Then I want go in stop mode for the remaining time which in this case is 3 seconds. Is ...

Frak.1 by Associate II
  • 2608 Views
  • 6 replies
  • 0 kudos

Resolved! SIGTRAP on ISR on "bare-metal" STM32F413ZH Nucleo-144

Hi guys, I'm a mechatronics student learning the basics of STM32s in my own time through the excellent series of guides by Vivonomicon. I'm currently learning interrupts, but my program seems to trigger a SIGTRAP fail when the interrupt fire.The code...

0693W00000QKmsKQAT.png
JFarr.4 by Associate II
  • 3098 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.