STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 understanding how UART data is transmitted

Hello. At the moment I am learning about STM32 and UART. I have configured UART4 and I am sending various data. I have connect logic analyzer on RX and TX pins are I am monitoring the signal.I send modbus write holding register message via the UART w...

0693W00000QNMQGQA5.png
LPetr.1 by Senior II
  • 6032 Views
  • 8 replies
  • 0 kudos

looking for SLC NAND flash driver for STM32F4 with FSMC

Hi I need to come up with a SLC NAND Flash Driver for STM32F405 which has a FSMC. My SLC NAND flash is ONFI 1.0 compliant (Micron MT29F). Any suggestion for a driver? Open source or commercial?I heared ST has one as well, but only available on reques...

MK..1 by Senior
  • 1420 Views
  • 1 replies
  • 0 kudos

How to differentiate between STM32H743 and H745 at runtime?

Is there any way to find out if the code is executed on a H743 (single core) or a H745 (dual core) MCU at runtime?If I am not mistaken the DBGMCU_IDC (Identity code register) has the same value for both MCUs. Is there any other register which I could...

CHild.1 by Associate
  • 3126 Views
  • 6 replies
  • 0 kudos

When to trigger an outage

当我�?�时打开uart的接�?�中断和�?�一uart dma的接�?�中断时,两个中断都会被触�?�,如果设置的优先级相�?�,触�?�的顺�?是什么?

pLI.1 by Associate
  • 905 Views
  • 1 replies
  • 0 kudos

Resolved! How to trim the STM32 HSI easily

HelloI'm using a stm32L431 with an STLinkV3https://www.st.com/en/microcontrollers-microprocessors/stm32l4x1.html#documentationHSI is enabled at 16MHz for USART2, used to receive a 1200Bd signal.I receive wrong characters because of the trim.I underst...

po221 by Senior
  • 6249 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.