STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cmake issue: Too many levels of symbolic links

Hi all!Currently, I create one project STM32F103 MCU with RTOS by Cmake and I got the issue when I compile the project. That is "Too many levels of symbolic links".My cmake version is 3.22.1.I would like to send you my CMakelists.txt file. Please che...

PTuan.1 by Associate
  • 1291 Views
  • 0 replies
  • 0 kudos

Resolved! About Pin function

I would like to do UART communication using nucleo l4r5zi.I would like to do the pin setting, but I do not know how to do that.​Please let me ask the following two questions here.1.Is my understanding correct that the pin settings for CN7, CN8, CN9 a...

Myasu.1 by Senior
  • 4980 Views
  • 2 replies
  • 0 kudos

DfuSe Demo v3.0.6 doesn't flash stm32f722ret6

I was trying to flash stm32f722ret6 via DFU mode. DfuSe Demo typing successful status but firmware doesn't update.But when I download .hex file via ST-LINK a firmware works. What could be the problem?

0693W00000QNm4kQAD.jpg 0693W00000QNm59QAD.jpg
ab.2 by Associate II
  • 4763 Views
  • 11 replies
  • 0 kudos

Error in writing RTC time & date into internal flash

Hello,I am working on a project in which i have to save my sensor readings in STM32G030F6's internal flash memory with time stamps. For that i am using STM's internal RTC to get the time and date. But problem is that i can't write data into flash if ...

Resolved! Is it possible on STM32H730 (or any) to switch between classical CAN and CANFD configurations during runtime?

I've been working on the STM32H730 processor and have been struggling to get the FDCAN peripherals to switch between classical CAN and CAN FD for transmissions. It seems that when I'm transmitting as classical CAN everything works fine. Then when I s...

0693W00000QNV0bQAH.png
snurb by Associate II
  • 2312 Views
  • 2 replies
  • 1 kudos

Resolved! NUCLEO L496ZG SWO not able to make it work

HiI am trying to enable the SWO to debug with printf. I have a NUCLEO L496ZG board. The ITM_SendChar function seems to get called but no data on the ITM console. What am I doing wrong?This is the main.c code:/** *************************************...

0693W00000QO4yRQAT.png 0693W00000QO4ybQAD.png 0693W00000QO4zFQAT.png 0693W00000QO53CQAT.jpg
RPG by Senior
  • 1767 Views
  • 3 replies
  • 0 kudos

STM32L082 - Dual NVM banks (how to boot from bank2)

Dear ST experts,I am using the STM32L082 and looking to utilize the Dual Banks to be able to upgrade the firmware (swap between bank1 and bank2 and visa versa). Have compiled code for BANK1 and compiled for BANK2. Code flashed to BANK1 (0x0800 0000) ...