STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to program STM32F407VET6 boards?

Hey everyone, I am new to STM hardware and software... Recently got a development board from a third party that's based around the aforementioned microcontroller. From what I gather you can start building on STM projects from STM32CubeMX, however I c...

STM32L4S9 UART Receive Problem.

Uart ConfigurationUart Receive CodeHello,I am working on a project with STM32L4S9 mcu and I am trying to receive data via uart from a GPS module (ublox CAM m8) which is continuously sending data. The problem is that when I am trying to debug with bre...

0693W00000SuOELQA3.png 0693W00000SuOEGQA3.png
SEfte.1 by Associate II
  • 3064 Views
  • 5 replies
  • 0 kudos

SDRAM Not working in STM32H757I-Eval Board.

I am using STM32H757I-Eval Board for our study, I created the project for STM32H757 SDRAM interface. While configuring the SDRAM through FMC. I configured SDRAM1 with Bank 2. After that found that the pin configuration generated by the code genera...

0693W00000StoijQAB.png

I2C Slave freezes SCL line

Hello,i tried to implement a I2C slave device on a STM32L486.It is working, but sometimes (after a few seconds, minutes or even hours) it freezes/blocks the SCL line. So the master device (also a STM32) generates a error.I have no glue what happens h...

Make USART6 as debug console in STM32F768-discovery board

Greetings !I am working on STM32F769 discovery board . I have built OS using Buildroot . I can able to get U-boot prompt through Default debug console (USART1).Here I having a requirement of changing default debug console (USART1) to USART6 . I am a...

PG.9 by Associate III
  • 2249 Views
  • 2 replies
  • 0 kudos

What is the max power consumption of the STM32L412RBT6?

Hello, I am estimating the max power consumption of the STM32L412RBT6. Based on the datasheet, I got two results, one is 303mW which is on page 78, and the other one is 0.462mW, which is on page 76( 3.3V X 140mA = 0.462mW). Please guide me on which o...

0693W00000SuSxZQAV.png 0693W00000SuSxoQAF.png
WChan.4 by Associate
  • 1733 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F746 Disco clear memory section

I Have STM32F746 Disco and i have a memory section that sould be initialized to zero.and the aim behind this is to keep the memory content whenever the board is rest.but unfortanlty, this section is being clear every time i restart the debuger.the se...

MFawzy by Associate III
  • 6105 Views
  • 11 replies
  • 1 kudos