STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Using STM32F723 I2C with multiple slaves at different voltages

Dear ST Microelectronics Team,I want to connect a STM32F723IE with I2C as master, which is powered with 3.0V, to a bus with one slave with 3.0V and to another slave with 3.8V. From the datasheet I can see that the GPIOs are 5V compliant, but can the ...

Rookie38 by Associate III
  • 1737 Views
  • 2 replies
  • 0 kudos

External crystal not oscillating

Hello,I have custom board. I am working on STM32H7 controller. We use the external crystal of 25Mhz. But when we use that external oscillator using the HSE ,it doesn't provide the clock to controller. Why these happening. Can you please help me

MDeva.1 by Associate II
  • 6644 Views
  • 10 replies
  • 0 kudos

STM32H750 and SDRAM signal groups

Need your advice. PCB routing. I have Divided signals into 4 groups + (CLK) : 1: Address: SDRAM_BA[0-1]/SDRAM_A[0-11] 2: Command: SDNRAS/SDNCAS/SDNWE 3: Control: NE0/CKE0/NBL[0-1] 4: Data: SDRAM_D[0-7] ( sub goup1 ) & [8-15] ( sub group 2) 5: SD...

BHell.1 by Associate II
  • 1293 Views
  • 1 replies
  • 0 kudos

SMBUS sample code for NUCLEO L496ZG

I am unable to find any working examples for this specific board with SMBUS/PMBUS.I am also having lot's of issues converting a SMBUS project from a different board.It would be great if anyone could assist me in either getting FW specific to the boar...

RENODE emulator vs. STM32L072 - how to "complete" MCU model?

Has anyone here worked with Renode? An emulator remotely similar to QEMU, but more geared towards MCUs, esp. w.r.t. emulating peripherals.https://antmicro.com/platforms/renode/Renode does not seem to have a forum, only the github issues for their pro...

SKled.1 by Senior II
  • 4092 Views
  • 0 replies
  • 0 kudos

How to properly configure ADC injected group?

Hello, I've tried to use ADC for two Potentiometers only with injected group conversion but couldn't make it work. I'm using STM32F446RE. I couldn't find solution so I'm asking here. Previously I read their value correctly via polling and I know that...

Where can I find the relation between the OSPEEDR register different value (Low, Medium, High and Very High) and the frequency of the signals I want to use?

Hello ST Microelectronics community,I'm using a STM32H743ZI and I'm currently working on configurating properly the different I/O I want to use.To do so I need to set the set the pull up/down, open drain,etc. And also the speed mode.I could not find ...

BNord.1 by Associate III
  • 3504 Views
  • 4 replies
  • 2 kudos