STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L031G6

I have a STM32L031G6 component in a UFQPN28 package, can I install a 3.68MHZ crystal, will it work or only in a UFQPN48 package

BPres.2 by Associate
  • 1009 Views
  • 1 replies
  • 0 kudos

Interruption, but corresponding interrupt flag is not set?

Dear community,I am having a strange problem with the STM32L431.The ADC is set up for use with both the DMA and interruption. This is to de-interleave the adc results from 2 different channels, since there was problem with interleaved ADC results whe...

0693W00000UoSQbQAN.png 0693W00000UoSQqQAN.png
ZJing by Associate III
  • 4644 Views
  • 10 replies
  • 0 kudos

Is there a way to tell whether ADC is busy? (STM32F303ve)

I am trying to reconfigure DMA without losing samples and without stopping the ADC, which is triggered using timer (relatively rarely), so my plan was to look whether both the ADC and DMA are idle and quickly reconfigure DMA before ADC even starts to...

SMisi by Associate II
  • 3466 Views
  • 6 replies
  • 1 kudos

Resolved! Unable to find pin B12 (BOOT0) on B-L47E-IOT01A2

Hi everyone,Something weird happened while I was uploading to my board. The upload crashed half way through and now the USB STLink interface isn't recognized. I think I should be able to upload a working ELF file in UART mode, but to do that I need t...

RBair.3 by Associate II
  • 1224 Views
  • 1 replies
  • 0 kudos

USART Receive to Idle DMA callbacks

I got this working, then it stopped working.I finally figured out after about 3 hours what is wrong.Situation. I am making a "Serial tap" for debugging. The STM32F411CE on the Black Pill board. 2xUSARTs Rx only and the CDC Virtual COM port device ...

PCamp.2 by Associate III
  • 5025 Views
  • 3 replies
  • 0 kudos