STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7+DMA+UART – which stream ?

Hi there,can anyone assist in understanding how to choose the correct ‘stream’ for an STM32H7 + DMA + UART setup, please ?I’m continuing work on a previous colleague’s firmware where UART1 was programmed to operate in DMA mode. This needs to change t...

TMA1of3 by Associate III
  • 3935 Views
  • 3 replies
  • 0 kudos

udp_client on stm32 h753 nuclio board

hii i have stm32 nucleo-h753 board and i finally managed to set the project in order to work with the ethernet port .i can ping the board successfully , so my next step is to send udp message from the board to my pc .i use herculis as my udp server ...

abeba.1 by Associate III
  • 911 Views
  • 0 replies
  • 0 kudos

Double precision computation

I'm using STM32F446xx 32-bit MCU, but I want to do computation using double precision. Is it possible to perform double computation precision using given MCU? And if so, how can I make sure that double computation is performed?

GOdin.1 by Associate
  • 1504 Views
  • 2 replies
  • 0 kudos

How to properly disable PWM on ST32L431?

I found that when after calling HAL_TIM_PWM_DeInit() the power consumption of the device is higher than it was before HAL_TIM_PWM_Init() called. The few investigations lead me to the fact that I need to reset ARR register to default value to reduce t...

Alex.Ag. by Associate II
  • 1335 Views
  • 1 replies
  • 0 kudos