User Activity

hi any one can help how to got sorce code stm32f334 for full bridge i need for design 10kw sic dc to dc this power not allowing on online desin st
how disable boot 0 pin8 i used this pin for input make problem to boot from flash how can disable any condition mcu boot from flash not check this pin when reset
how to make encoder siulation with timer
I USED 6 PCS TIMER IN ENCODER MODE NEED ON SOFTWARE 64BIT POSITION I USED CHECK DIR AND SR BIT FOR TRAKING BOUT SOME TIME CHANGE DIR FAST AND I MAKE MISTAKE AROUND 65535HOPE ANY ONE CAN HELP HOW TO RESOLVED void tasktim2(void){ uint16_t b2; if ((TIM2...
any one can help me how to used 2 pcs 16bit timer for make one 32bit on encoder mode need one example for setup timer