cancel
Showing results for 
Search instead for 
Did you mean: 

I have a B-L462E-CELL1 board, which has a CatM1/NB-IoT Type1SE modem. What I did: Put the SIM card, then connected the USB to the USB uart connector and sent the "AT" command, without a response. What am I missing?

MDuar.2
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14
CYANG.1
ST Employee

You can try to use User USB connector (CN8) or STlink USB connector (CN9) to check if there is a response.

jiangfan
ST Employee

it should be OK to connect USB-UART CN10;

select one of virtual COM port, with recognized message.

​configure with 115200,8,n1. no flow.

key in the Return Key, user should see the prompt character '>'. then you may input at command: "at at" and input Return, user should see expected response

0693W00000FC1p4QAD.gif

My CLI is disable

2 COM ports will be visible when USB-UART CN10 of B-L462E-CELL1 board is connected to PC, by default the CLI port should be enabled.

It shows disabled, and I press return key and nothing happens. How can I fix it?

0693W00000FD6aaQAD.png

You may try to recover to default configuration.

Get some binary or source files from x-cube-cellular website https://www.st.com/en/embedded-software/x-cube-cellular.html, then you can find the binary at (or similar location) STM32CubeExpansion_CELLULAR_V5.2.0\Projects\B_L462E\Demonstrations\Cellular\Binaries\l462_t1se_socket_v520.bin

I downloaded the x-cube-cellular and patch version 5.2.1, then flashed the binaries of the patch and x-cube folders, and the result was the same ( CLI disable). After I put the patch in the x-cube-cellular folder ( replacing the same files) and still not working. What could it be? 

In short, i tried the 3 binaries ( patch / x-cube / patch+x-cube) and didn´t work.

You may try with STlink USB connector (CN9) to check if there is a response. almost the same way, but better to set "local echo"

jiangfan
ST Employee

STlink USB connector (CN9) , at command response, for B-L462E-CELL1 board :

0693W00000FDOGiQAP.gif