STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why would UART_TX need to be set as OC with external pullup, if UART is set to single-wire half-duplex mode?

 Why?What happens if the respective pin is set as Push-Pull? And what happens if only the internal pullup is enabled and there's no external pullup?And there's no point to tell that the pin has to be set as "alternate function" - of course. That ST c...

0693W00000WHa5EQAT.png

Resolved! HAL_FLASH_Program trigger error 0x40 (FLASH_FLAG_SIZERR)

STM32G473CCT uses the HAL library for writing flash pages.i have constructed some code to use the last FLASH page as NV memory.bool eeprom_write8(uint16_t address, uint8_t data) { return eeprom_write(address, &data, 1); }   bool eeprom_write(uint16_...

0693W00000WHbqWQAT.png 0693W00000WHbt0QAD.png 0693W00000WHbsHQAT.png 0693W00000WHbs2QAD.png
sde c.1 by Senior II
  • 1522 Views
  • 1 replies
  • 0 kudos

Resolved! OTP size for STM32F746XX

I found a strange mismatch in the reference manual for the OTP memory size:Accordingly to the manual page 78 (https://www.st.com/resource/en/reference_manual/rm0385-stm32f75xxx-and-stm32f74xxx-advanced-armbased-32bit-mcus-stmicroelectronics.pdf) the ...

0693W00000WHcdNQAT.png
grmpyc8 by Associate
  • 1865 Views
  • 3 replies
  • 0 kudos

Pending Register for EXTI line 13 always active

Im trying some bare Metal programming on the NUCLEO - H743ZI2.Im stuck on creating a Button Interrupt on EXTI line 13.The User Button 1 is located on PC13, im trying to toggle LED2 on PE1.LED and Button configuration must be correct, since it works w...

J.v.W. by Associate II
  • 2746 Views
  • 7 replies
  • 0 kudos

STM32L011 in LP-RUN with STOP mode and RTC wakeup.

I would like to run the STM32L011K4 (Nucleo kit) in low power mode for 10ms then put it in STOP mode with a wake-up via the RTC 90ms later.Step 1: Operation in RUN mode all the time (10ms +90ms), the consumed current is about 54µA (57µA in DBG).Step ...