STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM input controlling PWM output

I have an interface that utilizes inverted PWM and I need a STM32F7 to receive and reply to messages from a controller. The controller sends 64 bit messages, the first 32 bits contains an address and if it matches with the address of the STM32F7, the...

Roth.Ian by Associate III
  • 1083 Views
  • 0 replies
  • 0 kudos

STM32 NUCLEO-F767ZI rs485

Hi i want to communicate between board with stm8 and board with stm32 the stm8 have rs485 communication bus does STM32 NUCLEO-F767ZI have build it in or i have to buy some extension?

uname.1 by Associate
  • 1457 Views
  • 1 replies
  • 0 kudos

Please can anyone show me a register that identifies the family "STM32F10x" of the MCU? I'm not interesting for a Unique device ID register "U_ID".

Hello,I would need a register that systematically identify the family type of the micro "STM32F103ZDT6".In the reference manual there is the Unique device ID register, but it gives a unique identifier to the chip, I would like an identifier that woul...

despo.1 by Associate
  • 2422 Views
  • 4 replies
  • 0 kudos

SDRAM Module Tester based on STM32F429

Hello everyone,I need to build a system to test a bunch of existing memory modules built around 512 Mbit SDRAM chips (4 chips each for total of 256 MBytes). The attached schematic shows the original design of the memory module and how it's connected ...

0693W00000WJDbGQAX.jpg
Zaher by Senior II
  • 1209 Views
  • 0 replies
  • 0 kudos

Multi-channel on STM32F429DISCO not working

Hello,I use a STM32F429DISCO REVE01 with a MCU STM32F429ZI.I have to use the ADC. On PA0, I connect a sensor with an amplifier and it's work, but when I want tu use ither channel like channel 1 with PA1 pin, that's not work, my value is around 0.Why ...

ABIZO.1 by Associate II
  • 1292 Views
  • 2 replies
  • 0 kudos

Debugging the MCU on a NUCLEO-H7A3ZI if 1.8V is selected?

Dear all,It seems like I actually broke two Nucleo 144 with a H7A3 and H723 after I tried to debug the MCU with the on board debugger and after switching the supply voltage for the MCU to 1.8V (no connection from debugger to MCU possible, even not wi...

Bench by Associate III
  • 1848 Views
  • 3 replies
  • 0 kudos