i tried to use the internal temperatur sensor but its a little bit strangewhen the tempertur goes up the value from the adc goes downis that right or is my config for the adc wrong ?
yes i did but the calculation i tried is wrongi think its much easier if the datasheet gives some examplesto start withfor example from the datasheet of a lm95071 this makes it clear how it has to be calculatedso can you tell me the hexvalue of the a...
do you have an example how to calculate the temperatur ?or which value whould by 0 °C ?the examples i found are only for other stm chips with 2 calibration values