STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F429ZI NUCLEO board that supports 6 SPI interfaces

I'm looking for an ARM based MCU that will handle IC configuration on a board in development. Really just need a full breakout for bench testing. I need it to handle at least 6 SPI lines. Comparing available NUCLEO boards to product selector I found ...

RMas by Associate II
  • 3543 Views
  • 5 replies
  • 0 kudos

Resolved! NUCLEO-U575 board, GPDMA destination address update problem

Hello everybody! So what I want to do, is to update the destination address (DAR) register of the DMA after the last transfer. So I write the desired destination address in a variable "dest_address", then I take the address of that variable and write...

Skfir by Senior
  • 1283 Views
  • 1 replies
  • 0 kudos

Resolved! Disabling memory Read Protection failed

Hello, we have boards with the MCU STM32F746. This works normally but in two cases we had a problem with the option bytes. Several values were changed and now we can't remove the protection.The first board we tried several times to change level prote...

GYacc by Associate II
  • 2745 Views
  • 2 replies
  • 0 kudos

I am looking the STM32L443CC Datasheet (DS11421 Rev 5 October 2019) and trying to figure out how you come up with the values for Table 66 Rain.

Doing my due diligence, I did find someone else asked the question in 2019 but there was no response.https://community.st.com/s/feed/0D50X0000BaM9PoSQK?t=1669134764953What it did show was the equation, but not where he found it, and no description of...

0693W00000WJFeqQAH.png 0693W00000WJFdsQAH.png
KiptonM by Lead
  • 2352 Views
  • 8 replies
  • 0 kudos

RAM code while erasing flash

Hi all,I'm trying to execute some code in interrupt mode (blinking a LED) while the MCU (STM32H725) is erasing a flash sector (obviously that is not used by the application). I've moved the vector table to RAM (0x240000000) and also the ISR function,...

Does anyone in the world have any information on how to get access to the "STPay-Topaz-Bio" biometric-enable cards? Do they exist? Is this yet more ST vapourware?

Ever time, I mean EVERY time I read an interesting link from ST about new tech, EVERYTIME it links to a product nobody has in stock, there are no reference designs, no support, no stock, no evaluation kits.This is such an inefficient way to operate a...

Multi Slave I2C Connection guidance

Hello,I have one master and multiple slave devices for I2C Connections.So, my Query is that;I am connecting series resistors after the Pull up Resistors on SDA SCL lines,Now the query is that should I connect those Series Resistors at only Master sid...

0693W00000WJwsWQAT.png
DBhut.1 by Senior
  • 1460 Views
  • 3 replies
  • 0 kudos